UI Name | Automation (neutral) Name | Value type | Range | Default Value | |||||
---|---|---|---|---|---|---|---|---|---|
Scratch Directory | Scratch Directory | integer |
|
CAE_DefaultNXMPScratchDirectory | |||||
Scratch Directory Location see note (1) |
Scratch Directory Location | string | -- | CAE_DefaultNXMPScratchDirectoryLocation | |||||
License Type | NastranLicenseType | integer |
|
CAE_DefaultNXMPNastranLicenseType | |||||
Input File Formatting | Input File Formatting | integer |
|
0 | |||||
Real Data Filter | Real Data Filter | boolean | true or false | false | |||||
Real Filter Value see note (2) |
Real Filter Value | double | 0.000 to FLT_MAX | 1e-015 | |||||
Use environment variable UGII_NX_NASTRAN | Use Environment Solver Executable | boolean | true or false | CAE_DefaultNXMPNastranSolverEnv | |||||
User Specified see note (3) |
solver executable | string | -- | CAE_DefaultNXMPNastranSolverLocation | |||||
Use environment variable UGII_NX_NASTRAN_VERSION | Use Environment Solver Version | boolean | true or false | CAE_DefaultNXMPNastranVersionEnv | |||||
User Specified see note (4) |
solver version | string | -- | CAE_DefaultNXMPNastranVersionUser | |||||
Solution Monitor | solution monitor | boolean | true or false | false | |||||
Solution Summary Tab for Legacy Monitor see note (5) |
solution summary tab | boolean | true or false | CAE_DefaultSolutionSummaryTab | |||||
Open Core Memory to Allocate | memory | string | -- | CAE_DefaultNXMPNastranSolverMemory | |||||
Save Previous Copies of the Output Files | old | boolean | true or false | true | |||||
Delete Database Files | scratch | integer |
|
0 | |||||
Enable Shared-Memory Parallel | Enable Shared-Memory Parallel | boolean | true or false | true | |||||
Maximum Number of CPUs see note (6) |
Maximum Number of CPUs | integer | 1to 1 | 1 | |||||
Additional Keywords | additional keywords | string | -- | CAE_DefaultNXMPNastranAdditionalKeywords | |||||
Run Solution in Parallel | Run Solution in Parallel | boolean | true or false | true | |||||
Parallel Configuration File see note (7) |
Parallel Configuration File | string | -- | CAE_DefaultNXMPParallelConfigurationFile | |||||
Enable Multithreading | Enable Multithreading | boolean | true or false | true | |||||
Number of Execution Threads see note (8) |
Number of Execution Threads | integer | 1to 1 | CAE_DefaultNXMPNumberThreads |